Property (Read-Write)
SCPI.SENSe(Ch).BWAuto.LIMit.RESolution = Value
Value = SCPI.SENSe(Ch).BWAuto.LIMit.RESolution
This command sets/gets maximum IF bandwidth in bandwidth auto mode, for the selected channel (Ch).
|
Parameter |
Value |
|
Description |
maximum IF bandwidth in bandwidth auto mode |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
1 to 3E+5 |
|
Preset Value |
3E+4 |
|
Unit |
Hz |
Dim BWALim as Double
SCPI.SENSe(4).BWAuto.LIMit.RESolution = 3E+4
BWALim = SCPI.SENSe(4).BWAuto.LIMit.RESolution
Avg > IFBW Auto Limit
:SENSe{[1]-4}:BWAuto:LIMit[:RESolution] <numeric>
:SENSe{[1]-4}:BWAuto:LIMit[:RESolution]?
{numeric} <newline><^END>
10 OUTPUT 717;":SENS1:BWA:LIM 1E+5"
20 OUTPUT 717;":SENS1:BWA:LIM?"
30 ENTER 717;A