Property (Read-Write)
SCPI.SENSe(Ch).DC.MEASure.ENABle = Status
Status = SCPI.SENSe(Ch).DC.MEASure.ENABle
This command turns ON/OFF DC monitor measurement on sweep end, for the selected channel ( Ch).
|
Parameter |
Status |
|
Description |
ON/OFF the DC monitor measurement on sweep end. |
|
Data Type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset Value |
False or OFF |
Dim StatDCmon as Boolean
SCPI.SENSe(1).DC.MEASure.ENABle = True
StatDCmon = SCPI.SENSe(1).DC.MEASure.ENABle
Meas > DC Monitor Setup > DC Monitor On Sweep End > Monitor
:SENSe{[1]-4}:DC:MEASure:ENABle {ON|OFF|1|0}
:SENSe{[1]-4}:DC:MEASure:ENABle?
{1|0} <newline><^END>
10 OUTPUT 717;":SENS1:DC:MEAS:ENAB ON"
20 OUTPUT 717;":SENS1:DC:MEAS:ENAB?"
30 ENTER 717;A