Property (Read-Write)
SCPI.SENSe(Ch).Z.METHod = Value
Value = SCPI.SENSe(Ch).Z.METHod
This command sets or gets the impedance method.
When the method changes, the Fixture Compensation table is cleared.
|
Parameter |
Value |
|
Description |
Impedance method |
|
Data Type |
Character string type (String) |
|
Range |
Select one of the following options: P1Reflection:S-Parameter Port 1 reflection measurement (for simple impedance measurement) P2Reflection:S-Parameter Port 2 reflection measurement (for simple impedance measurement) TSERies:S-Parameter series-through measurement (for simple impedance measurement) TSHunt:S-Parameter shunt-through measurement (for PDN component characterization) GSERies:Gain-Phase series-through measurement (for simple impedance measurement) GSHunt:Gain-Phase shunt-through measurement (for PDN component characterization) |
|
Preset Value |
P1Reflection |
|
Unit |
- |
|
Resolution |
- |
Dim Var as String
Var= "P1Reflection"
SCPI.SENSe(1).Z.METHod = Var
Var = SCPI.SENSe(1).Z.METHod
There is no equivalent key is available on the front panel. However, the similar key is:
Meas > Method > Port 1 Refl OR
Meas > Method > Port 2 Refl OR
Meas > Method > Port 1-2 Series OR
Meas > Method > Port 1-2 Shunt OR
Meas > Method > GP Series T 50W R 1MW OR
Meas > Method > GP Shunt T 50W R 50W
:SENSe{[1]-4}:Z:METHod <string>
:SENSe{[1]-4}:Z:METHod?
<string><newline><^END>
10 OUTPUT 717;":SENS1:Z:METH P1R"
20 OUTPUT 717;":SENS1:Z:METH?"
30 ENTER 717;A$