Method (Write Only)
SCPI.SENSe(Ch).CORRection.COEFficient.METHod.RESPonse.SHORt = Port
This command sets the calibration type to the response calibration (short) of the specified port for the selected channel, when the calibration coefficient data array is written with the SCPI.SENSe(Ch).CORRection.COEFficient.DATA command.
See Port.
SCPI.SENSe(1).CORRection.COEFficient.METHod.RESPonse.SHORt = 1
SCPI.SENSe(Ch).CORRection.COEFficient.DATA
SCPI.SENSe(Ch).CORRection.COEFficient.SAVE
No equivalent key is available on the front panel.
:SENSe{[1]-4}:CORRection:COEFficient:METHod[:RESPonse]:SHORt <numeric>
10 OUTPUT 717;":SENS1:CORR:COEF:METH:SHOR 1"