Property (Read-Write)
SCPI.SENSe(Ch).SEGMent.DATA = Data
Data = SCPI.SENSe(Ch).SEGMent.DATA
This command creates the segment sweep table of the selected channel ( Ch).
|
Parameter |
Data |
|
Description |
Indicates the array data arranged in the following order (for the segment sweep table); where N is the number of segments (specified with <segm>) and n is an integer between 1 and N. Data = {<buf>,<stim>,<ifbw>,<pow>,<del>,<time>,<segm>, <star 1>,<stop 1>,<nop 1>,<ifbw 1>,<pow 1>,<del 1>,<time 1>,... , <star n>,<stop n>,<nop n>,<ifbw n>,<pow n>,<del n>,<time n>,.... , <star N>,<stop N>,<nop N>,<ifbw N>,<pow N>,<del N>,<time N>} Each parameter in the above array data is detailed below:
|
|
Data type |
Variant type (Variant) |
|
Note |
If the necessary amount of array data for the specified number of segments is not available while setting the segment sweep table, an error occurs when its executed and the object is ignored. For <stim>, <ifbw>, <pow>, <del>, and <time>, if the specified value is not the allowable integer, an error occurs when its executed. For <star n>, <stop n>, <nop n>, <ifbw n>, <pow n>, <del n>, and <time n> in the array data, if the specified value is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim SegmData As Variant
SCPI.SENSe(1).SEGMent.DATA = Array(5,0,0,1,0,0,2, _
100E6,1E9,31,0,2E9,3E9,51,-10)
SegmData = SCPI.SENSe(1).SEGMent.DATA
Dim SegmData(14) As Variant
Dim Ref As Variant
SegmData(0) = 5
SegmData(1) = 0
SegmData(2) = 0
SegmData(3) = 1
SegmData(4) = 0
SegmData(5) = 0
SegmData(6) = 2
SegmData(7) = 100E6
SegmData(8) = 1E9
SegmData(9) = 31
SegmData(10) = 0
SegmData(11) = 2E9
SegmData(12) = 3E9
SegmData(13) = 51
SegmData(14) = -10
SCPI.SENSe(1).SEGMent.DATA = SegmData
Ref = SCPI.SENSe(1).SEGMent.DATA
Sweep Setup > Edit Segment Table
:SENSe{[1]-4}:SEGMent:DATA 5,<mode>,<ifbw>,<pow>,<del>,<time>,<segm>,
<star 1>,<stop 1>,<nop 1>,<ifbw 1>,<pow 1>,<del 1>,<time 1>,... ,
<star n>,<stop n>,<nop n>,<ifbw n>,<pow n>,<del n>,<time n>,... ,
<star N>,<stop N>,<nop N>,<ifbw N>,<pow N>,<del N>,<time N>
:SENSe{[1]-4}:SEGMent:DATA?
Where N is the number of segments (specified with <segm>) and n is an integer between 1 and N.
5,{mode},{ifbw},{pow},{del},{time},{segm},
{star 1},{stop 1},{nop 1},{pow 1},{del 1},{time 1},... ,
{star n},{stop n},{nop n},{pow n},{del n},{time n},... ,
{star N},{stop N},{nop N},{pow N},{del N},{time N}<newline><^END>
10 DIM H(1:3,1:4)
20 OUTPUT 717;":SENS1:SEGM:DATA 5,0,1,0,0,0,3,";
30 OUTPUT 717;"1E9,3E9,11,70e3,";
40 OUTPUT 717;"3E9,4E9,51,7e3,";
50 OUTPUT 717;"4E9,6E9,11,70e3"
60 OUTPUT 717;":SENS1:SEGM:DATA?"
70 ENTER 717;A,B,C,D,E,F,G,H(*)