Property (Read Only)
Value = SCPI.SERVice.SWEep.FREQuency.MAXimum
This command reads the upper limit of measurement frequency of E5061B.
|
Parameter |
Value |
|
Description |
Upper limit of measurement frequency |
|
Data type |
Double precision floating point type (Double) |
Dim MaxFreq As Double
MaxFreq = SCPI.SERVice.SWEep.FREQuency.MAXimum
No equivalent key is available on the front panel.
:SERVice:SWEep:FREQuency:MAXimum?
{numeric}<newline><^END>
10 OUTPUT 717;":SERV:SWE:FREQ:MAX?"
20 ENTER 717;A