Property (Read-Write)
SCPI.SOURce.BIAS.ENABle = Status
Status = SCPI.SOURce.BIAS.ENABle
This command turns ON/OFF the DC bias output.
Measurement cannot be made until the DC bias output is turned ON.
|
Parameter |
Status |
|
Description |
ON/OFF of the stimulus signal output |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset value |
False or OFF |
Dim StatBias as Boolean
SCPI.SOURce.BIAS.ENABle = True
StatBias = SCPI.SOURce.BIAS.ENABle
Sweep Setup > DC Bias
System > Overload Recovery > DC Bias
:SOURce:BIAS:ENABle {ON|OFF|1|0}
:SOURce:BIAS:ENABle?
{1|0} <newline><^END>
10 OUTPUT 717;":SOUR:BIAS:ENAB ON"
20 OUTPUT 717;":SOUR:BIAS:ENAB?"
30 ENTER 717;A