Property (Read-Write)
SCPI.SOURce(Ch).POWer.STOP = Value
Value = SCPI.SOURce(Ch).POWer.STOP
This command sets/gets the stop value of the power sweep for the selected channel (Ch).
|
Parameter |
Value |
|
Description |
Stop value |
|
Data type |
Double precision floating point type (Double) |
|
Range |
–45 to 10 dBm |
|
Preset value |
0 |
|
Unit |
dBm |
|
Resolution |
0.05 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Pstop As Double
SCPI.SOURce(1).POWer.STOP = 10
Pstop = SCPI.SOURce(1).POWer.STOP
Stop
:SOURce{[1]-4}:POWer:STOP <numeric>
:SOURce{[1]-4}:POWer:STOP?
{numeric}<newline><^END>
10 OUTPUT 717;":SOUR1:POW:STOP 10"
20 OUTPUT 717;":SOUR1:POW:STOP?"
30 ENTER 717;A