Property (Read-Write)
SCPI.STATus.QUEStionable.LIMit.NTRansition = Value
Value = SCPI.STATus.QUEStionable.LIMit.NTRansition
This command sets/gets the value of the negative transition filter of the Questionable Limit Status Register.
|
Parameter |
Value |
|
Description |
Value of the negative transition filter |
|
Data type |
Long integer type (Long) |
|
Range |
0 to 65535 |
|
Preset value |
0 |
|
Note |
The bit 0, and bit 5 to 15 can not be set to 1. |
Dim Stat As Long
SCPI.STATus.QUEStionable.LIMit.NTRansition = 6
Stat = SCPI.STATus.QUEStionable.LIMit.NTRansition
SCPI.STATus.QUEStionable.LIMit.EVENt
SCPI.STATus.QUEStionable.LIMit.PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:LIMit:NTRansition <numeric>
:STATus:QUEStionable:LIMit:NTRansition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:LIM:NTR 16"
20 OUTPUT 717;":STAT:QUES:LIM:NTR?"
30 ENTER 717;A