SCPI.SYSTem.PRESet

Object type

Method (Write Only)

Syntax

SCPI.SYSTem.PRESet

Description

This command presets the setting state of the E5061B to the original factory setting ( Default Conditions). This command is different from SCPI.IEEE4882.RSTas the continuous startup mode (see SCPI.INITiate(Ch).CONTinuous) of channel 1 is set to ON.

Examples

SCPI.SYSTem.PRESet

Related objects

SCPI.IEEE4882.RST

Equivalent key

Preset > OK

Equivalent SCPI command

Syntax

:SYSTem:PRESet

Example of use

10 OUTPUT 717;":SYST:PRES"