Property (Read-Write)
SCPI.TRIGger.SEQuence.POINt = Status
Status = SCPI.TRIGger.SEQuence.POINt
This command turns ON/OFF or returns the status of the point trigger feature.
When the trigger source is set to the internal trigger (Internal), the setting is ignored.
|
Parameter |
Status |
|
Description |
Turns ON/OFF the point trigger |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from either of the following: True or ON: Turns ON the point trigger. False or OFF: Turns OFF the point trigger. |
|
Preset value |
False or OFF |
Dim Ptrig As Boolean
SCPI.TRIGger.SEQuence.POINt = True
Ptrig = TRIGger.SEQuence.POINt
Trigger > Trigger Event
:TRIGger[:SEQuence]:POINt {ON|OFF|1|0}
:TRIGger[:SEQuence]:POINt?
{1|0}<newline><^END>
10 OUTPUT 717;":TRIG:POIN ON"
20 OUTPUT 717;":TRIG:POIN?"
30 ENTER 717;A