Other topics about Setting up Analyzer
When you set the number of traces, that setting determines the upper limit trace number; for example, if the setting is 3, traces 1 through 3 are displayed. To set the number of traces, use the following command:
:CALC{1-4}:PAR:COUN
Only the currently displayed traces can be active traces. Therefore, you must set the number of traces appropriately before making them active.
To select the measurement parameter (S parameter) for each trace, use the following command:
:CALC{1-4}:PAR{1-4}:DEF
There is no equivalent command with Meas > Measurement Port. Using this command allows you to select the parameters for Gain-Phase and S-Parameter measurements in one channel. (For example, Trace 1: T/R, Trace 2: S11).
To select one of the above sweep types, use the following command:
:SENS{1-4}:SWE:TYPE
To turn ON/OFF the stimulus signal output, use the following command:
:OUTP
To set the sweep range, use the following commands:
|
Type |
Command |
|
Start value |
:SENS{1-4}:FREQ:STAR |
|
Stop value |
:SENS{1-4}:FREQ:STOP |
|
Center value |
:SENS{1-4}:FREQ:CENT |
|
Span value |
:SENS{1-4}:FREQ:SPAN |
To set the number of measurement points, use the following command:
:SENS{1-4}:SWE:POIN
To set the sweep time, use the following commands:
|
Type |
Command |
|
Sweep time |
:SENS{1-4}:SWE:TIME |
|
Turning ON/OFF auto setting |
:SENS{1-4}:SWE:TIME:AUTO |
To set the sweep delay time, use the following command:
:SENS{1-4}:SWE:DEL
To set the IF bandwidth, use the one of the following commands (both provide the same function):
:SENS{1-4}:BAND
:SENS{1-4}:BWID
To set the AUTO IF bandwidth, use the following command:
:SENS{1-4}:BWA
To set the power level, use the following command:
:SOUR{1-4}:POW
To select whether to output the same power level (the set value for port 1) or a different power level for each port, use the following command:
:SOUR{1-4}:POW:PORT:COUP
:SOUR{1-4}:POW:PORT{1-2}
When you opt to use segment sweep, you can set all items (in the segment sweep table) by using a single command:
:SENS{1-4}:SEGM:DATA
Alternatively, you can configure the segment sweep settings based on the data contained in a CSV file by issuing the following command:
:MMEM:LOAD:SEGM
Also, you can save the contents of the current segment sweep table to a file by issuing the following command:
:MMEM:STOR:SEGM
For more information on how to save and load the segment sweep table, refer to Saving and recalling the segment sweep table.
To set the sweep range, use the following commands:
|
Type |
Command |
|
Start value |
:SOUR{1-4}:POW:STAR |
|
Stop value |
:SOUR{1-4}:POW:STOP |
|
Center value |
:SOUR{1-4}:POW:CENT |
|
Span value |
:SOUR{1-4}:POW:SPAN |
To set the fixed frequency (CW frequency), use the following command:
:SENS{1-4}:FREQ
To set the number of points, the sweep time, the sweep delay time, and the IF bandwidth, use the same commands as for the linear/log sweep.
To configure the averaging settings, use the following commands:
|
Type |
Command |
|
On/off |
:SENS{1-4}:AVER |
|
Averaging factor |
:SENS{1-4}:AVER:COUN |
|
Clear (Restart) |
:SENS{1-4}:AVER:CLE |
For averaging, normally, the instrument must be triggered according to the number of averaging; however, when the averaging trigger is turned ON, sweeps for the number of averaging can be executed by a single trigger. For details on the averaging trigger, refer to Averaging Trigger Function.
To set the system characteristic impedance (Z0), use the following command:
:SENS:CORR:IMP