Selecting the Active Channel/Trace

You can configure the E5061B by using various commands. Some commands require you to specify and work with a particular channel or trace, while other commands do not have this restriction.

Those commands that do not require you to specify a particular channel or trace apply to the currently active channels and traces. Before issuing such a command, therefore, you must make the appropriate channels and traces active.

To make a channel active, use the following command:

:DISP:WIND{1-4}:ACT

To make a trace active, use the following command:

:CALC{1-4}:PAR{1-4}:SEL

Other topics about Setting up Analyzer