An Overview of a Control System Based on the Macro Function

Other topics about Introduction to VBA Programming

Overview

This section describes how you can use the E5061B's built-in VBA macro function to implement a system that controls the E5061B and peripherals, and what command sets are available for such purposes.

Implementing a Control System

Macro-based control systems are classified into two types: As shown in the following figure, a VBA control system controls the E5061B itself while a VBA remote control system controls peripherals. When you use the macro function to control the peripherals, you must connect the E5061B with the peripherals through USB/GPIB interface, USB or LAN, and configure them to communicate over VISA (Virtual Instrument Software Architecture). For information on programming using the VISA library, refer to Programming with VISA.

Configuration example of control system using macro environment

Required Equipment

Control Methods

The command set you can use differs depending on whether you use the macro function to control the E5061B or a peripheral.

Controlling the E5061B

When you want to control the E5061B itself, you can create a program using COM objects within the E5061B VBA environment. COM objects that come with the E5061B include seven objects specific to the COM interface and COM objects that correspond to SCPI commands.

Controlling a Peripheral

When you want to control a peripheral, you can create a program using VISA library functions within the E5061B VBA environment.

For information on using the VISA library, see Controlling Peripherals. For a complete description on VISA functions, refer to the VISA library's online help.

For information on the GPIB commands that is available with a particular peripheral, refer to the documentation that comes with the peripheral.