Value = FirstRightGap(Chan)
Returns the response difference between the fist detected positive peak when searching from the left edge toward the right edge within the analysis range and its right adjacent negative peak.
FirstRightGap

|
Parameter |
Chan |
|
Description |
Specifies the channel number. |
|
Data type |
Integer type (Integer) |
|
Range |
1 to 9 |
|
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
|
Parameter |
Value |
|
Description |
Returns the response difference between the first detected positive peak when searching from the left edge toward the right edge within the analysis range and its right adjacent negative peak. |
|
Data type |
Double precision floating point type (Double) |
|
Note |
If no applicable point is detected, 0 is returned. |
Dim Value As Double
Value = FirstRightGap(1)
MsgBox "First Right Gap =" & Value