The E5061B has the built-in clock that keeps track of the date and time. This clock is used for the following functions.
To display the current date and time in the instrument status bar at the lower part of the screen
To write date and time information when saving internal data or a VBA program
The Date & Time of E5061B clock can be changed by double-clicking the clock at the bottom right of the taskbar.