The differences in Windows display is due to the Windows licenses used with the storage revision.
The license label at rear panel is Windows Vista Business.
The Windows task bar is shown at the bottom of the screen.
The license label at rear panel is Windows XP Pro for Embedded Systems.
The license label at rear panel is Windows Embedded Standard 7.
The Windows task bar is shown at the bottom of the screen.
The license label at rear panel is Windows 10.
The Windows task bar is shown at the bottom of the screen.
The Windows resizing buttons are shown at the upper-right of the Windows titlebar. There is no E5061B resize button at the upper-right of the channel titlebar.
The Windows re-sizing buttons are no longer appear at the upper-right of the Windows titlebar. It is replaced with E5061B resize button at the upper-right of the channel titlebar, as shown in the following figure:

![]()