Unknown Thru Calibration

Other topics about Advanced Calibration

Overview

Unknown Thru Cal is the preferred THRU method of calibrating the E5063A to measure a non-insertable device. The major benefits of using a unknown Thru calibration are:

The Thru must satisfy the following requirements:

  1. Thru must be Reciprocal (with S21 and S12 equal) in nature. It should have a consistent behavior, independent of the direction from which it is used.

  2. The electrical length of the Thru should be known at an accuracy of ±1 /4 of the wavelength.

  3. Unknown Thru is NOT supported during the TRL calibration.

Procedure

To measure the nominal electrical delay of the Unknown Thru standard:

  1. With port 1 configured, perform a simple S11 response calibration at port 1 by using a short circuit.

    Press Cal > Calibrate > Response (Short) > Short.

  2. Connect the Unknown Thru standard to port 1 and terminate the standard with a short circuit.

  3. Measure the electrical delay of the Unknown Thru standard.

    Press Cal > Port Extensions > Auto Port Extension > Measure SHORT > Port 1.

    The electrical delay is automatically measured and can be confirmed.

    Press Cal > Port Extensions > Extension Port 1 {Value}.

  4. If there is an offset in the short circuit used to terminate the Unknown Thru standard, remember to subtract its electrical length from the measurement result.

To perform the unknown Thru Calibration, follow the procedure below:

  1. Press Cal > Calkit , then select the desired calibration kit (e.g. 85033D or User Kit).

  2. Press Cal > Modify Cal Kit > Define STDs > No Name > Label.

  3. Type a name for unknown Thru Cal standard e.g. {Unknown Thru1}.
  4. Press Cal > Modify Cal Kit > Define STDs > {Defined Name} > STD Type > Unknown Thru.

  5. Click Offset Delay, then enter the approximate offset delay value of the unknown Thru standard.

  6. Press Cal > Modify Cal Kit > Specify CLSs > Thru > Port 1-2 > {Defined Name}.

  7. Press Cal > Calibrate > 2-Port Cal > Transmission > {Defined Name} to execute mechanical Unknown Thru calibration.

  8. Complete Reflection, and Isolation (optional) calibration for 2 full port Cal.