ECal Driver Installation

When the ECal is connected t USB ports at the first time, ECal driver installation is required.

  1. Connect an ECal to the USB port of the E5063A.

  2. "Keysight USB ECal Module : Device driver software installed successfully" message box prompts at the right end of the task bar.

  3. ECal is now ready to be used.

Other topics about Calibration with ECal