Calibration Types and Characteristics

The table shows the different types of calibrations and the features of each method.

Calibration Method

Standard (s) Used

Corrected Error Factor

Measurement Parameters

Characteristics

No calibration

None

None

All parameters

  • Low accuracy

  • Calibration not required

Response Calibration

Following 2 error terms:

S11(Reflection characteristics at 1 port)

  • Medium-level accuracy

  • Quick calibration

  • Isolation calibration improves the accuracy in a reflection measurement of a DUT with high return loss

Following 2 error terms:

S21
(1 direction transmission characteristics at 2 ports)

  • Medium-level accuracy

  • Quick calibration

  • Isolation calibration improves the accuracy in a transmission measurement of a device with high insertion loss

1-Port Calibration

ECal module (2-port/4-port)

Following 3 error terms:

  • Directivity (Ed)

  • Source Match (Es)

  • Reflection Tracking (Er)

S11
(Reflection characteristics at 1 port)

  • 1-port measurement with the highest degree of accuracy

  • Quick calibration with low chance of operator error

  • OPEN

  • SHORT

  • LOAD

  • Highly accurate 1-port measurement

Enhanced Response Calibration

Ecal module (2-port/4-port)

Following 5 error terms:

  • Directivity (Ed1)

  • Isolation (Ex21)

  • Source Match (Es1)

  • Transmission Tracking (Et21)

  • Reflection Tracking (Er1)

S11, S21 (1 direction transmission/Reflection characteristics at 2 ports)

  • OPEN

  • SHORT

  • LOAD

  • THRU

Full 2-Port Calibration

ECal module (2-port/4-port)

Following 12 error terms:

  • Directivity (Ed1,Ed2)

  • Isolation (Ex21,Ex12)

  • Source Match (Es1,Es2)

  • Load Match (El12,El21)

  • Transmission Tracking (Et21,Et12)

  • Reflection Tracking (Er1,Er2)

S11,S21,S12,S22
(All S-parameters at 2 ports)

  • OPEN

  • SHORT

  • LOAD

  • THRU

2-Port TRL Calibration

  • Reflection (OPEN or SHORT)

  • THRU

  • LINE

  • MATCH

Following 12 error terms:

  • Directivity (Ed1,Ed2)

  • Source Match (Es1,Es2)

  • Load Match (El1,El2)

  • Transmission Tracking
    (Et21,Et12)

  • Reflection Tracking
    (Er1,Er2)

S11,S21,S12,S22
(All S-parameters at 2 ports)

Other topics about Calibration