Other topics about Making Measurement
The averaging trigger function is used to execute the sweep the number of times specified by the averaging factor with a single trigger when the sweep averaging function is ON.
|
Averaging Trigger |
Function |
|
ON |
Performs the sweep the number of times specified by the averaging factor with a single trigger. |
|
OFF |
Performs the sweep once with a single trigger. |
The averaging factor is cleared before the start of measurement.
When the point trigger function is ON, its setting has priority, and you need to generate triggers based on "(number of measurement points) × (averaging factor)".
When the sweep averaging function is OFF, sweep is performed only once even if the averaging trigger function is set to ON.
The averaging trigger function is valid for all the channels. Note that you can set the sweep averaging function for each channel.
When the sweep averaging function is ON, follow these steps to set the averaging trigger function.
Press Avg > Avg Trigger.
Click ON to activate the averaging trigger.
Press Trigger.
Click Single. The averaging factor is cleared before the start of measurement, the sweep is executed the number of times specified by the averaging factor, and then the instrument waits for the next trigger.