The E5063A creates automatic log of data for troubleshooting purpose. The log files are stored in both SSD and flash memory. For security reasons, if this data needs to be deleted, then :SERV:LOGG:CLE (SSD) and :SERV:LOGG:ERAS (Flash memory) commands can be used to clear the log recorded by the E5063A. It is necessary to execute both commands to erase the log data.
The log file stores data related to:
Power ON time
Number of times of power ON
Result of power ON test
Number of times of overload
Event Log
Hardware driver installation/error Log
Connected USB device Log
User calibration Log
Firmware error Log
Temperature of analog boards
Internal test result