Command/Query
:CALCulate<Ch>[:SELected]:DATA:SDATa <Value>
:CALCulate<Ch>[:SELected]:DATA:SDATa?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:DATA:SDATa <Value>
:CALCulate<Ch>:TRACe<Tr>:DATA:SDATa?
This command sets/gets the corrected data array.
The array data element varies in the data format. For more information, see Internal Data Processing.
If valid data is not calculated because of the invalid measurement, “1.#QNB” is read out.
|
Parameter |
Value |
|
Description |
Corrected data array Where n is an integer between 1 and NOP (number of measurement points):
The number of data is {NOP×2} |
|
Data Type |
Variant type Array (Range) |
|
Note |
If there is no array data of NOP×2 when setting a formatted data array, an error occurs when executed. |
{numeric 1}, .... ,{numeric NOP×2}<newline><^END>
See Reading/Writing Data.
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.DATA.SDATA
SCPI.CALCULATE(Ch).TRACE(Tr).DATA.SDATA