Command/Query
:CALCulate<Ch>[:SELected]:FILTer[:GATE]:DISTance[:TYPE] {BPASs|NOTCh}
:CALCulate<Ch>[:SELected]:FILTer[:GATE]:DISTance[:TYPE]?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:FILTer[:GATE]:DISTance[:TYPE] {BPASs|NOTCh}
:CALCulate<Ch>:TRACe<Tr>:FILTer[:GATE]:DISTance[:TYPE]?
This command sets/gets the gate type used for the gating function of the fault location display.
|
Parameter |
Selection Option |
|
Description |
The gate type |
|
Data Type |
Character string type (String) |
|
Range |
"BPASs": Band-pass type. "NOTCh": Notch type. |
|
Preset Value |
"BPASs" |
{BPAS|NOTC}<newline><^END>
Dim Var as String
Var= "BPASs"
Ena.WriteString ":CALC1:FILT:DIST " & Var, True
Ena.WriteString ":CALC1:FILT:DIST?", True
Var=Ena.ReadString
Analysis > Gating > Type
SCPI.CALCULATE(Ch).SELECTED.FILTER.GATE.DISTANCE.TYPE
SCPI.CALCULATE(Ch).TRACE(Tr).FILTER.GATE.DISTANCE.TYPE