Command/Query
:CALCulate<Ch>[:SELected]:FILTer[:GATE]:TIME:STATe {ON|OFF|1|0}
:CALCulate<Ch>[:SELected]:FILTer[:GATE]:TIME:STATe?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:FILTer[:GATE]:TIME:STATe {ON|OFF|1|0}
:CALCulate<Ch>:TRACe<Tr>:FILTer[:GATE]:TIME:STATe?
This command turns ON/OFF the gating function of the time domain function. When the X axis is distance (Meters, Feet or Inches), use :CALC:FILT:DIST:STAT.
This command is available for option 010/011 only.
You can turn ON the gating function only when the sweep type is the linear sweep and the number of points is 3 or more. If this turns ON when the sweep type is other than linear sweep or the number of points is less than 3, an error occurs and this is ignored.
|
Parameter |
Selection Option |
|
Description |
ON/OFF of the gating function |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
{1|0}<newline><^END>
Dim Var as Integer
Var = 1
Ena.WriteString ":CALC1:FILT:TIME:STAT " & Str(Var), True
Ena.WriteString ":CALC1:FILT:TIME:STAT?", True
Var=Ena.ReadNumber
Analysis > Gating > Gating
SCPI.CALCULATE(Ch).SELECTED.FILTER.GATE.TIME.STATE
SCPI.CALCULATE(Ch).TRACE(Tr).FILTER.GATE.TIME.STATE