Command/Query
:CALCulate<Ch>:FSIMulator:SENDed:PMCircuit:PORT<Pt>:USER:FILename <String>
:CALCulate<Ch>:FSIMulator:SENDed:PMCircuit:PORT<Pt>:USER:FILename?
This command specifies the file in which the information on the user-defined matching circuit is saved (2-port touchstone file).
Specify the file name with the extension. When you use directory names (folder names) and file name, separate them with "\ " (back slash), or "/" (slash).
Even if the specified file does not exist, no error occurs when you execute this command. However, when you set the type of the matching circuit to the user-defined circuit with the :CALC:FSIM:SEND:PMC:PORT, an error occurs.
|
Parameter |
String |
|
Description |
2-port touchstone file name (extension: .s2p) for the matching circuit |
|
Data Type |
Character string type (String) |
|
Range |
254 chars |
|
Preset Value |
"" |
{String}<newline><^END>
Dim Var as String
Var = "D:\Myfile.s2p"
Ena.WriteString ":CALC1:FSIM:SEND:PMC:PORT1:USER:FIL " & Var, True
Ena.WriteString ":CALC1:FSIM:SEND:PMC:PORT1:USER:FIL?", True
Var=Ena.ReadString
Analysis > Fixture Simulator > Port Matching > User File...
SCPI.CALCULATE(Ch).FSIMULATOR.SENDED.PMCIRCUIT.PORT(Pt).USER.FILENAME