:CALC<Ch>:FUNC:EXEC

Type

Command

Syntax

:CALCulate<Ch>[:SELected]:FUNCtion:EXECute

 

The following syntax is also supported:

:CALCulate<Ch>:TRACe<Tr>:FUNCtion:EXECute

Description

This command executes the analysis function.

Examples

See Peak Search.

Related Commands

:CALC:PAR:SEL

:CALC:FUNC:DATA

:CALC:FUNC:TYPE

:CALC:FUNC:DOM

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.CALCULATE(Ch).SELECTED.FUNCTION.EXECUTE

SCPI.CALCULATE(Ch).TRACE(Tr).FUNCTION.EXECUTE