Command
:CALCulate<Ch>[:SELected]:LIMit:OFFSet:MARKer
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:LIMit:OFFSet:MARKer
This command sets the active marker value to amplitude offset using the limit line. The setting of the limit line does not change even if the offset value is changed. When the markers are not displayed, this command does not operate.
Ena.WriteString ":CALC1:LIM:OFFS:MARK", True
Analysis > Limit Test > Limit Line Offsets > Marker > Amplitude Offset
SCPI.CALCULATE(Ch).SELECTED.LIMIT.OFFSET.MARKER
SCPI.CALCULATE(Ch).TRACE(Tr).LIMIT.OFFSET.MARKER