Command/Query
:CALCulate<Ch>[:SELected]:MARKer<Mk>:FUNCtion:PEXCursion <Value>
:CALCulate<Ch>[:SELected]:MARKer<Mk>:FUNCtion:PEXCursion?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:FUNCtion:PEXCursion <Value>
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:FUNCtion:PEXCursion?
This command sets/gets the limit of peak excursion value.
|
Parameter |
Value |
|
Description |
Lower limit of peak excursion value |
|
Data Type |
Numeric type (Real) |
|
Range |
0 to 500M |
|
Preset Value |
3 |
|
Unit |
Varies depending on the data format. Log magnitude (MLOG): dB (decibel) Phase (PHAS), Expanded phase (UPH) or Positive phase (PPH): × (degree) Group delay (GDEL): s (second) Others: No unit |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
{numeric}<newline><^END>
See Peak Search.
Marker Search > Peak > Peak Excursion
SCPI.CALCULATE(Ch).SELECTED.MARKER.FUNCTION.PEXCURSION
SCPI.CALCULATE(Ch).TRACE(Tr).MARKER.FUNCTION.PEXCURSION