Command/Query
:CALCulate<Ch>[:SELected]:MARKer<Mk>:FUNCtion:PPOLarity {POSitive|NEGative|BOTH}
:CALCulate<Ch>[:SELected]:MARKer<Mk>:FUNCtion:PPOLarity?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:FUNCtion:PPOLarity {POSitive|NEGative|BOTH}
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:FUNCtion:PPOLarity?
This command sets/gets the polarity of the peak search with marker 1 to 9 and reference marker for the selected channel <Ch>.
|
Parameter |
Selection Option |
|
Description |
Polarity for peak search |
|
Data Type |
Character string type (String) |
|
Range |
Select from the following: POSitive: Positive peak. NEGative: Negative peak. BOTH: Both the positive peak and the negative peak. |
|
Preset Value |
POSitive |
{POS|NEG|BOTH}<newline><^END>
See Peak Search.
Marker Search > Peak > Peak Polarity
SCPI.CALCULATE(Ch).SELECTED.MARKER.FUNCTION.PPOLARITY
SCPI.CALCULATE(Ch).TRACE(Tr).MARKER.FUNCTION.PPOLARITY