Command
:CALCulate<Ch>[:SELected]:MARKer<Mk>:SET {CENTer|STARt|STOP|RLEVel|DELay}
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:SET {CENTer|STARt|STOP|RLEVel|DELay}
This command sets the value at the position of marker 1 to 9 (Mk) and reference marker (Mk:10) to the value of the instrument setting item (Param).
|
Parameter |
Selection Option |
|
Description |
Instrument setting item |
|
Data Type |
Character string type (String) |
|
Range |
"STARt": Sets the sweep start value to the stimulus value at the marker position. "STOP": Sets the sweep stop value to the stimulus value at the marker position. "CENTer": Sets the sweep center value to the stimulus value at the marker position. "RLEVel": Sets the reference line value to the response value at the marker position. "DELay": Sets the electrical delay time value to the value of the group delay at the marker position (a value smoothed with the aperture of 20%). |
Dim Var as String
Var= "CENTer"
Ena.WriteString ":CALC1:MARK1:SET & Var, True
Marker Fctn > Marker > Start
Marker Fctn > Marker > Stop
Marker Fctn > Marker > Center
Marker Fctn > Marker > Reference
Marker Fctn > Marker > Delay
SCPI.CALCULATE(Ch).SELECTED.MARKER(Mk).SET
SCPI.CALCULATE(Ch).TRACE(Tr).MARKER(Mk).SET