Command/Query
:CALCulate<Ch>[:SELected]:MARKer<Mk>:X <Value>
:CALCulate<Ch>[:SELected]:MARKer<Mk>:X?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:X <Value>
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:X?
This command set the stimulus value for marker 1 to 9 (Mk) and reference marker (Ch:10).
|
Parameter |
Value |
|
Description |
Stimulus value of the marker |
|
Data Type |
Numeric type (Real) |
|
Range |
Sweep start value to sweep stop value |
|
Preset Value |
100k |
|
Unit |
Hz (hertz), s (second), m (meter), ft (feet) or in (inches) |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
{numeric}<newline><^END>
Dim Var as Double
Ena.WriteString ":CALC1:MARK1:X" & Str(Var), True
Ena.WriteString ":CALC1:MARK1:X?", True
Var=Ena.ReadNumber
Marker > Marker 1 | Marker 2 | Marker 3 | Marker 4
Marker > More Markers > Marker 5 | Marker 6 | Marker 7 | Marker 8 | Marker 9
When performing the operation from the front panel, turn ON the marker and set the stimulus value at the same time.
SCPI.CALCULATE(Ch).SELECTED.MARKER(Mk).X
SCPI.CALCULATE(Ch).TRACE(Tr).MARKER(Mk).X