Command/Query
:CALCulate<Ch>:PARameter<Tr>:DEFine {S11|S21|S12|S22}
:CALCulate<Ch>:PARameter<Tr>:DEFine?
This command sets/gets the measurement parameter.
|
Parameter |
Selection Option |
|
Description |
Measurement parameter |
|
Data Type |
Character string type (String) |
|
Range |
Select either one of the following:
Where: x=1 to 2 Y=1 to 2 |
|
Preset Value |
"S11" |
{S11|S21|S12|S22}<newline><^END>
Dim Var as String
Var= "S11"
Ena.WriteString ":CALC1:PAR1:DEF " & Var, True
Ena.WriteString ":CALC1:PAR1:DEF?", True
Var=Ena.ReadString
Measurement > Measurement > S11|S21|S12|S22
Analysis > Fixture Simulator > Measurement > S11|S21|S12|S22
SCPI.CALCULATE(Ch).PARAMETER(Tr).DEFINE