Query
:CALCulate<Ch>[:SELected]:PLIMit:FAIL?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:PLIMit:FAIL?
This command returns true if point limit test has failed..
{1|0}<newline><^END>
1: fail, 0: pass
Dim Var as String
Ena.WriteString ":CALC1:PLIM:FAIL?", True
Var=Ena.ReadNumber
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.PLIMIT.FAIL