Command/Query
:CALCulate<Ch>[:SELected]:RLIMit:DATA <Value>
:CALCulate<Ch>[:SELected]:RLIMit:DATA?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:RLIMit:DATA <Value>
:CALCulate<Ch>:TRACe<Tr>:RLIMit:DATA?
This command sets/gets list for ripple limit test. if n bands, #_of_data=1+4*n. The first data must be 4*n., for the selected channel Ch.
|
Parameter |
Value |
|
Description |
Indicates the array data (for ripple line) of 1 + Num (number of limit lines)* 4. Where n is an integer between 1 and Num.
Specify an integer 0 to 1 as follows. 0: OFF 1: ON
The index of the array starts from 0. |
|
Data Type |
Variant type Array (Range) |
|
Note |
If there is no array data of 1+Num (number of set lines))×4 when setting a formatted memory array, an error occurs when executed and the object is ignored. For Data(n×4-3) in the array data, if you specify an integer other than 0 or 1, an error occurs when executed. For Data(n×4-2) and Data(n×4-1) in the array data, if the specified value is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
{numeric 1 (N:number of limit lines)}, ... , {numeric 1+(Nx4)}<newline><^END>
This sample requires manual modification
Dim Var(1 to 49) as Variant
Ena.WriteString ":CALC1:RLIM:DATA" & Var(), True
Ena.WriteString ":CALC1:RLIM:DATA?", True
Var=Ena.ReadList(ASCIIType_R8, ",")
Analysis > Ripple Limit > Edit Ripple Limit
SCPI.CALCULATE(Ch).SELECTED.RLIMIT.DATA
SCPI.CALCULATE(Ch).TRACE(Tr).RLIMIT.DATA