:CALC<Ch>:TRAN:TIME:LPFR

Type

Command

Syntax

:CALCulate<Ch>[:SELected]:TRANsform:TIME:LPFRequency

 

The following syntax is also supported:

:CALCulate<Ch>:TRACe<Tr>:TRANsform:TIME:LPFRequency

Description

This command changes the frequency range to match with the low-pass type transformation of the transformation function of the time domain function. Use:CALC:TRAN:DIST:LPFR when :CALC:TRAN:METH is set at distance.

Examples

Ena.WriteString ":CALC1:TRAN:TIME:LPFR", True

Related Commands

:CALC:TRAN:METH

:CALC:TRAN:TIME:STAT

 

:CALC:TRAN:TIME

:CALC:TRAN:TIME:STIM

:CALC:TRAN:TIME:IMP:WIDT

:CALC:TRAN:TIME:KBES

 

:CALC:TRAN:TIME:CENT

:CALC:TRAN:TIME:SPAN

:CALC:TRAN:TIME:STAR

:CALC:TRAN:TIME:STOP

 

:CALC:TRAN:DIST:LPFR

Equivalent Softkey

Analysis > Transform > Set Freq Low Pass

COM Command Syntax (Internal Control Only)

SCPI.CALCULATE(Ch).SELECTED.TRANSFORM.TIME.LPFREQUENCY

SCPI.CALCULATE(Ch).TRACE(Tr).TRANSFORM.TIME.LPFREQUENCY