Command/Query
:CONTrol:HANDler:D[:DATA] <Value>
:CONTrol:HANDler:D[:DATA]?
When input/output port D of the handler I/O is set to the output port, it outputs port information to output port D (D0 to D3).
When input/output port D of the handler I/O is set to the input port, it reads out port information to input to port D (D0 to D3).
Port information is output as 4-bit binary data using D0 as LSB and D3 as MSB.
|
Parameter |
Value |
|
Description |
Port information (input/output) |
|
Data Type |
Numeric type (Integer) |
|
Range |
0 ~ 15 |
{numeric}<newline><^END>
Dim Var as Long
Var= 0
Ena.WriteString ":CONT:HAND:D" & Str(Var), True
Ena.WriteString ":CONT:HAND:D?", True
Var=Ena.ReadNumber
No equivalent key is available on the front panel.
SCPI.CONTROL.HANDLER.D.DATA