*OPC

Type

Command/Query

Syntax

*OPC

*OPC?

Description

This command sets/gets the operation complete (OPC) bit (bit 0) of the Standard Event Status Register. When all of pending operations complete, *OPC returns 1.

Variable

Query Response

{1}<newline><^END>

Examples

Dim Var as Integer
Ena.WriteString "*OPC?", True
Var=Ena.ReadNumber

Related Commands

*CLS

*ESE

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.IEEE4882.OPC