Command
*RST
This command presets the E5063A to its default settings and is different from setting state preset with the SCPI.SYSTem.PRESet object as the continuous initiation mode (see SCPI.INITiate(Ch).CONTinuous) of channel 1 is set to OFF.
Ena.WriteString "*RST", True
No equivalent key is available on the front panel.
SCPI.IEEE4882.RST