*TST

Type

Query

Syntax

*TST?

Description

Does nothing. The self-test is not executed by this command in the case of the E5063A. Always returns 0.

Variable

Query Response

{0}<newline><^END>

Examples

Dim Var as Integer
Ena.WriteString "*TST?", True
Var=Ena.ReadNumber

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.IEEE4882.TST