Command
:INITiate<Ch>[:IMMediate]
This command changes the state of each channel to the initiation state in the trigger system.
When this command is executed for a channel in the idle state in the trigger system, it goes into the initiation state immediately. Then, after measurement is executed once, it goes back to the idle state.
If this command is executed for a channel that is not in the idle state or a channel for which the continuous initiation mode is set to ON (setting by which the trigger system initiates continuously) in the trigger system, an error occurs when executed and the object is ignored.
Ena.WriteString ":INIT", True
Trigger > Single (When :INIT:CONT is OFF.)
SCPI.INITIATE(ch).IMMEDIATE