|
Parameter |
Value |
|
Description |
The loss value of DC. |
|
Data type |
Double precision floating point type (Double) |
|
Range |
-90 to 90 |
|
Preset value |
0 |
|
Unit |
dBm |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |