Command
:SENSe<Ch>:CORRection:COLLect:ADAPter<Pt>:ROTate
This command executes Adapter Removal/Insertion along with moving the phase of adapter (which is removed or inserted) to 180 degrees. This command is useful in cases where auto judgement of phase fails. This command can be executed several times while the calibration remains valid.
If user cannot execute this command, then "Execution error" is displayed.
Ena.WriteString ":SENSe:CORRection:COLLect:ADAPter:ROTate", True
Cal > Calibrate > Adapter Removal > Rotate Adapter
SCPI.SENSE(Ch).CORRECTION.COLLECT.ADAPTER(Pt).ROTATE