:SENS<Ch>:CORR:COLL:ECAL:CCH

Type

Command

Syntax

:SENSe<Ch>:CORRection:COLLect:ECAL:CCHeck[:ACQuire]

Description

This command executes the confidence check of the calibration coefficients using ECal (Electronic Calibration).  In other words, this command sets the data measured with the analyzer and the data stored in ECal so that they can be compared).

      • If you execute this object when the ECal module is not connected or when ports are not connected each other appropriately, a runtime error occurs.

Examples

Ena.WriteString ":SENS1:CORR:COLL:ECAL:CCH", True

Equivalent Softkey

Calibration > ECal > Confidence Check

COM Command Syntax (Internal Control Only)

SCPI.SENSE(Ch).CORRECTION.COLLECT.ECAL.CCHECK.ACQUIRE