:SENS<Ch>:CORR:COLL:PART:SAVE

Type

Command

Syntax

:SENSe<Ch>:CORRection:COLLect:PARTial:SAVE

Description

This command, used for partial overwrite, recalculates the calibration coefficients depending on the selected calibration type from the measured calibration data.

Calculating the calibration coefficients clears all calibration data regardless of whether they are used for the calculation and also clears the calibration type selections.

If partial overwrite is executed before selecting the calibration type, an error occurs and the command is ignored.

Examples

Ena.WriteString ":SENS:CORR:COLL:PART:SAVE", True

Related Commands

Equivalent Softkey

Cal > Calibrate > {n-Port Cal} > Overwrite

COM Command Syntax (Internal Control Only)

SCPI.SENSE(Ch).CORRECTION.COLLECT.PARTIAL.SAVE