Query
:SENSe:ROSCillator:SOURce?
This command reads whether the external reference signal is inputted to the Ref In connector on the rear panel
|
Parameter |
Selection Option |
|
Description |
Whether the external reference signal is inputted or not |
|
Data Type |
Character string type (String) |
|
Range |
INTernal: Internal |
{INT|EXT}<newline><^END>
Dim Var as String
Ena.WriteString ":SENS:ROSC:SOUR?", True
Var=Ena.ReadString
Displayed on the instrument status bar (at the bottom of the LCD display).
SCPI.SENSE(Ch).ROSCILLATOR.SOURCE