Command/Query
:STATus:QUEStionable:BLIMit:CHANnel<Ch>:ENABle <Value>
:STATus:QUEStionable:BLIMit:CHANnel<Ch>:ENABle?
This command sets/gets the value of the "Questionable Bandwidth Limit Channel Status Enable Register" for the specified channel.
The bit 0, and bit 5 to 15 cannot be set to 1.
|
Parameter |
Value |
|
Description |
Value of the enable register |
|
Data Type |
Numeric type (Integer) |
|
Range |
0 ~ 65535 |
|
Preset Value |
0 |
{0 ~ 65535}<newline><^END>
Dim Var as Long
Var= 0
Ena.WriteString ":STAT:QUES:BLIM:CHAN1:ENAB" & Str(Var), True
Ena.WriteString ":STAT:QUES:BLIM:CHAN1:ENAB?", True
Var=Ena.ReadNumber
No equivalent key is available on the front panel.
SCPI.STATUS.QUESTIONABLE.BLIMIT.CHANNEL(Ch).ENABLE