Command/Query
:SYSTem:COMMunicate:SWITch<Sw>:DEFine <String>
:SYSTem:COMMunicate:SWITch<Sw>:DEFine?
This command sets/gets the USB switch information (<Sw>: 1 or 2). .
|
Parameter |
String |
|
Description |
USB switch |
|
Data Type |
Character string type (String) |
|
Range |
254 chars |
|
Preset Value |
"" |
{String}<newline><^END>
Dim Var as String
Ena.WriteString ":SYST:COMM:SWIT:DEF " & Var, True
Ena.WriteString ":SYST:COMM:SWIT:DEF?", True
Var=Ena.ReadString
No equivalent key is available on the front panel.
SCPI.SYSTEM.COMMUNICATE.SWITCH(Sw).DEFINE