Command/Query
:TRIGger[:SEQuence]:POINt {ON|OFF|1|0}
:TRIGger[:SEQuence]:POINt?
This command turns ON/OFF or returns the status of the point trigger feature.
When the trigger source is set to the internal trigger (Internal), the setting is ignored.
|
Parameter |
Selection Option |
|
Description |
Turns ON/OFF the point trigger |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
{1|0}<newline><^END>
Dim Var as Integer
Var = 1
Ena.WriteString ":TRIG:POIN " & Str(Var), True
Ena.WriteString ":TRIG:POIN?", True
Var=Ena.ReadNumber
Trigger > Trigger Event
SCPI.TRIGGER.SEQUENCE.POINT