Command/Query
:DISPlay:ATRaces:SCALe:RPOSition {LEFT|CENTer}
:DISPlay:ATRaces:SCALe:RPOSition?
This command sets x-axis reference position.
|
Parameter |
Selection Option |
|
Description |
Sets x-axis reference position |
|
Data Type |
Character string type (String) |
|
Range |
LEFT: The reference position is left edge CENTer: The reference position is center |
|
Preset Value |
LEFT |
{LEFT|CENT}<newline><^END>
Dim Var as String
Var= "LEFT"
Ena.WriteString ":DISP:ATR:SCAL:RPOS " & Var, True
Ena.WriteString ":DISP:ATR:SCAL:RPOS?", True
Var=Ena.ReadString
Edit Test > Test Limit >
or
(Under Horizontal Scale)